TCPIP_SNMP_TRAPMibIDGet Function

C

void TCPIP_SNMP_TRAPMibIDGet(
    uint32_t * mibID
);

Description

This function is used to get the MIB ID which is require while transmitting SNMP notification.This MIB ID is a Agent ID value of the Microchip style MIB script. MIB ID macro value is present in mib.h which is generated by mib2bib.jar.

Preconditions

TCPIP_SNMP_Initialize() is already called.

Parameters

ParametersDescription
mibIDTrap client MIB ID.

Returns

None.

Remarks

None.