11 Revision History

The revision history describes the changes that were implemented in the document. The changes are listed by revision, starting with the most current publication.

Table 11-1. Revision History
RevisionDateDescription
E05/2025The following is a summary of the changes made in revision E of this document.
D09/2023The following is a summary of the changes made in revision D of this document.
C09/2022The following is a summary of the changes made in revision C of this document.
B05/2021

The following is a summary of the changes made in revision B of this document.

A03/2021

The following is a summary of the changes made in revision A of this document.

  • The document was migrated to the Microchip template.
  • The document number was updated to DS60001692A from 50200902.
  • Updated Table 1-1 .
  • Updated Table 1-2.
  • Updated Table 1-3 .
  • Updated Table 1-6 .
2.0—

The following is a summary of the changes made in revision 2.0 of this document.

  • Updated MSS I/Os. Added refer to PolarFire SoC Packaging Pin Assignment Table for the pin out information for the MSS pins.
  • Deleted Unused Condition columns from all the details. Added refer to UG0901: PolarFire SoC FPGA Board Design Guidelines User Guide.
  • Added LPDDR4 memory in DDR Interface.
  • Updated Dedicated I/O Bank Pins. Added UG0901: PolarFire SoC FPGA Board Design Guidelines User Guide.
  • Updated XCVR Interface. Added UG0901: PolarFire SoC FPGA Board Design Guidelines User Guide.
1.0—

Initial Release.