3.6.4.13.2 Serial Bridge Application to Upgrade ATWINC1510 Firmware
Description
This application acts as a serial bridge between the PC utility (winc1510_firmware) and the ATWINC1510 module on WiFi 7 click board.
The application interfaces with the PC over UART and with the WiFi 7 click (ATWINC1510 module) board over the SPI lines.
The application receives the ATWINC1510 firmware from the PC, and programs it into the ATWINC1510 module (on WiFi 7 click board).
Hardware Used
Software/Tools Used
This project has been verified to work with the following versions of software tools:
Because Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected. It is recommended to double-check and use the same versions that the project was tested with.
Setup
- Mount SAM E51 Curiosity Nano Evaluation Kit on CNANO56_HOST_CONN (U3) connector of Curiosity Nano Base board.
- Mount WiFi 7 Click board on mikroBUS click 1 connector of Curiosity Nano Base board.
- Connect a USB cable to
the DEBUG USB port for programming.
Programming Hex File
The pre-built hex file can be programmed by following the below steps.
- Open MPLAB X IDE
- Close all existing projects in IDE, if any project is opened
- Go to File -> Import -> Hex/ELF File.
- In the Import Image File
window,
- Create Prebuilt
Project,
- Click the Browse button to select the prebuilt hex file in "winc1510_firmware_upgrade_serial_bridge/hex" folder.
- Select Device as ATSAME51J20A.
- Ensure the proper tool is selected under Hardware Tool and click on Next button.
- Select Project Name and
Folder,
- Select appropriate project name and folder and click on Finish button
- Create Prebuilt
Project,
- In MPLAB X IDE, click on Make and Program Device button to program the device.
- Follow the steps in Running the Demo section below.
Running the Demo
- Ensure the board is powered on (a USB cable is connected to the DEBUG USB port).
- Refer the Running the Demo section in the documentation under utility/readme file. Click Here.
Comments
- How to Setup MPLAB Harmony v3 Software Development Framework (DS90003232).
- How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project (DS90003253).
- MPLAB Harmony v3 is configurable through MPLAB Code Configurator (MCC). Refer to the below links for specific instructions to use MPLAB Harmony v3 with MCC.