3.6.4.13.1 ATWINC1510 Firmware Upgrade Guide
Description:
This Application uses the WiFi 7 click board (containing Microchip's ATWINC1510-MR210PB IEEE 802.11 b/g/n module) to enable cloud connectivity. The application's functioning requires the ATWINC1510 module to have firmware compatible with the WiFi software stack running on the ATSAME51 microcontroller(on SAM E51 Curiosity Nano Development Kit). To enable this compatibility, the ATWINC1510 module is updated with the firmware compatible with WiFi software running in the latest released demo.
Running the utility
- Download and extract same51_winc_upgrader into utilities folder
- Open command prompt and navigate to "utilities/same51_winc_upgrader"
- The following command line will
generate a device programming file winc1500_19.7.7.prog.
image_tool.exe -c winc1500_19.7.7\config.txt -o winc1500_19.7.7.prog -of prog
- The file produced can be used to
upgrade a WINC1500 to version 19.7.7 including the firmware, HTTP files and
root
certificates.
- The following command line will
program a WINC1500 device via the serial port
winc_programmer -p COM8 -d winc1500 -i winc1500_19.7.7.prog -if prog -w -r -pfw winc1500_19.7.7\firmware\programmer_firmware.bin
Attention: Respective device COM PORT should be selected in above command and all other serial terminal application should be closed -
Wait till verify passed message comes up as shown below