14.5 Call Stack Window
Select to open the Call Stack window. You must be in debug mode to view content.
The Call Stack window displays C functions and their arguments listed in the order in which they were called in the executing program. C code that is not optimized works best.
The Call Stack is available for 16- and 32-bit devices. The window is updated on Debug Pause or Halt.

The following icons are available on the window on Pause or Halt.
| Icon | Description |
|---|---|
![]()
| Auto or Manual
Refresh of Window Contents. Depends on the value of Disable auto
refresh for call stack view during debug sessions under – Unchecked = false (default), checked = true. See Generic Settings Tab. False = Auto Refresh (Green Icon): The window contents are automatically updated on Pause or Halt. If the window is closed or not focused, selecting the window and clicking this button will display the updates without having to run and pause/halt again. True = Manual Refresh (Orange Icon): The window contents are not automatically updated on Pause or Halt. This button must be clicked to update window contents on a pause/halt. |
![]() | Select to disable/enable evaluation of function parameter variables. |
![]() | Change visible columns. For this window, show or hide location of call stack frame. |