16.3.2.3 Command Modes
Reading the memory arrays is handled using the LD*/LPM(*) instructions.
Erasing the entire Flash (CHER) or EEPROM (EECHER) is
started by writing commands to the Control A (CTRLA) register. The other write/erase
operations are only enabled by writing commands to the CTRLA register and must be followed
by writes using ST*/SPM(*)
instructions to the memory arrays.
Note: *
LPM/SPM cannot be used for EEPROM.
The following sequence must execute to write a command in the CTRLA register:
- Confirm that any previous operation is completed by reading the Busy (EEBUSY and FBUSY) flags in the STATUS register.
- Write the appropriate key to the Configuration Change Protection (CPU.CCP) register to unlock the Control A (NVMCTRL.CTRLA) register.
- Write the desired command value to the CMD bit field in the Control A (NVMCTRL.CTRLA) register within the following four instructions.
Note: Skipping the first step will trigger an error in the
Status (NVMCTRL.STATUS) register if an operation is still ongoing when issuing a new
command.
The following steps are required to perform a write/erase operation in the NVM:
- Confirm that any previous operation is completed by reading the Busy (EEBUSY and FBUSY) flags in the STATUS register.
- Optional: If accessing the Flash in the CPU data space, map the corresponding 32 KB Flash section into the data space by writing the FLMAP bit field in the CTRLB register.
- Write the desired command value to the CTRLA register as described before.
- Write to the correct address in the data space/code space using the ST*/SPM instructions.
- Optional: If multiple write operations are required, go to step 4.
- Write a NOOP or NOCMD command to the CTRLA register to clear the current command.