1.1.3.4.9 DRV_MEMORY_SyncEraseWrite Function
C
bool DRV_MEMORY_SyncEraseWrite
(
const DRV_HANDLE handle,
void *sourceBuffer,
uint32_t blockStart,
uint32_t nBlock
);Summary
Erase and Write data for the specified number of memory blocks in Synchronous mode.
Description
This function combines the step of erasing a sector and then writing the page. The application can use this function if it wants to avoid having to explicitly delete a sector in order to update the pages contained in the sector.
This function schedules a blocking operation to erase and write blocks of data into attached device memory.
Precondition
The DRV_MEMORY_Open() must have been called with DRV_IO_INTENT_WRITE or DRV_IO_INTENT_READWRITE as a parameter to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open function |
| sourceBuffer | The source buffer containing data to be programmed into media device memory |
| blockStart | block start where the write should begin. |
| nBlock | Total number of blocks to be written. |
Returns
- true
- If the transfer request is successfully completed.
- false
- If the sourceBuffer pointer is NULL
- If the client opened the driver for read only
- If the number of blocks to be written is either zero or more than the number of blocks actually available
- If the driver handle is invalid
Example
#define BUFFER_SIZE 4096 uint8_t buffer[BUFFER_SIZE]; // Use DRV_MEMORY_GeometryGet () to find the write region geometry. uint32_t blockStart = 0x0; uint32_t nBlock = BUFFER_SIZE / block_size; // block_size for write geometry // memoryHandle is the handle returned by the DRV_MEMORY_Open function. if(DRV_MEMORY_SyncEraseWrite(memoryHandle, &myBuffer, blockStart, nBlock) == false) { // Error handling here }
Remarks
This API is supported only in RTOS environment.