1.1.3.4.18 DRV_MEMORY_IsAttached Function
C
bool DRV_MEMORY_IsAttached
(
const DRV_HANDLE handle
);Summary
Returns the physical attach status of the Media.
Description
This function returns the physical attach status of the Media device.
Precondition
The DRV_MEMORY_Open() routine must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open function |
Returns
Returns false if the handle is invalid otherwise returns true.
Example
bool isMEMORYAttached; isMEMORYAttached = DRV_MEMORY_isAttached(drvMEMORYHandle);
Remarks
None.