1.1.3.4.20 DRV_MEMORY_AddressGet Function
C
uintptr_t DRV_MEMORY_AddressGet
(
const DRV_HANDLE handle
);Summary
Returns the Memory media start address
Description
This function returns the Memory Media start address.
Precondition
The DRV_MEMORY_Open() routine must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open function |
Returns
Start address of the Memory Media if the handle is valid otherwise NULL.
Example
uintptr_t startAddress; startAddress = DRV_MEMORY_AddressGet(drvMEMORYHandle);
Remarks
None.