1.1.3.4.7 DRV_MEMORY_SyncErase Function
C
bool DRV_MEMORY_SyncErase
(
const DRV_HANDLE handle,
uint32_t blockStart,
uint32_t nBlock
);Summary
Erase the specified number of memory blocks in Synchronous mode.
Description
This function schedules a blocking sector erase operation for the specified number of memory blocks from the specified block start start address on attached memory device.
Preconditions
The DRV_MEMORY_Open() must have been called with DRV_IO_INTENT_WRITE or DRV_IO_INTENT_READWRITE as a parameter to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open function |
| blockStart | block start from where the blocks should be erased. |
| nBlock | Total number of blocks to be erased. |
Returns
true
- If the transfer request is successfully completed.
false
- If the client opened the driver for read only
- If the number of blocks to be erased is either zero or more than the number of blocks actually available
- If the driver handle is invalid
Example
// Use DRV_MEMORY_GeometryGet () to find the erase region geometry. uint32_t blockStart = 0; uint32_t nBlocks = 10; // memoryHandle is the handle returned by the DRV_MEMORY_Open function. if(DRV_MEMORY_SyncErase( memoryHandle, blockStart, nBlock ) == false) { // Error handling here }
Remarks
This API is supported only in RTOS environment..