1.1.3.4.24 DRV_MEMORY_Read Function
C
void DRV_MEMORY_Read
(
const DRV_HANDLE handle,
SYS_MEDIA_BLOCK_COMMAND_HANDLE* commandHandle,
void* sourceBuffer,
uint32_t blockStart,
uint32_t nBlock
)Summary
Interface to the file system to perform a read operation in Synchronous mode
Description
This routine provides interface to the file system to perform a media read operation in synchronous mode of the Memory driver.
Preconditions
The DRV_MEMORY_Open must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open function |
| commandHandle | Pointer to an argument that will contain the return buffer handle |
| sourceBuffer | The source buffer containing data to be programmed to the SD Card. |
| blockStart | Start block address of SD Card where the writes should begin. |
| nBlock | Total number of blocks to be written. |
Returns
The buffer handle is returned in the commandHandle argument. It will be DRV_MEMORY_COMMAND_HANDLE_INVALID if the request was not successful.
Remarks
This function is internally used by the file system and should not be used by application.