1.1.3.4.19 DRV_MEMORY_IsWriteProtected Function
C
bool DRV_MEMORY_IsWriteProtected
(
const DRV_HANDLE handle
);Summary
Returns the write protect status of the Memory.
Description
This function returns the write protect status of the Memory.
Precondition
The DRV_MEMORY_Open() routine must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open function |
Returns
True - If the memory is write protected.
False - If the memory is not write protected.
Example
bool isWriteProtected; isWriteProtected = DRV_MEMORY_IsWriteProtected(drvMEMORYHandle);
Remarks
None.