1.1.3.4.32 DRV_MEMORY_DEVICE_INTERFACE Struct
C
/* Function pointer typedef to open the attached media */
typedef DRV_HANDLE (*DRV_MEMORY_DEVICE_OPEN)( const SYS_MODULE_INDEX drvIndex, const DRV_IO_INTENT ioIntent );
/* Function pointer typedef to close the attached media */
typedef void (*DRV_MEMORY_DEVICE_CLOSE)( const DRV_HANDLE handle );
/* Function pointer typedef to erase a sector from attached media */
typedef bool (*DRV_MEMORY_DEVICE_SECTOR_ERASE)( const DRV_HANDLE handle, uint32_t address);
/* Function pointer typedef to get the status of the attached media */
typedef SYS_STATUS (*DRV_MEMORY_DEVICE_STATUS)( const SYS_MODULE_INDEX drvIndex );
/* Function pointer typedef to read from the attached media */
typedef bool (*DRV_MEMORY_DEVICE_READ)( const DRV_HANDLE handle, void *rx_data, uint32_t rx_data_length, uint32_t address );
/* Function pointer typedef to write a page to the attached media */
typedef bool (*DRV_MEMORY_DEVICE_PAGE_WRITE)( const DRV_HANDLE handle, void *tx_data, uint32_t address );
/* Function pointer typedef to get the Geometry details from attached media */
typedef bool (*DRV_MEMORY_DEVICE_GEOMETRY_GET)( const DRV_HANDLE handle, MEMORY_DEVICE_GEOMETRY *geometry );
/* Function pointer typedef to get the transfer Status from attached media */
typedef uint32_t (*DRV_MEMORY_DEVICE_TRANSFER_STATUS_GET)( const DRV_HANDLE handle );
/* Function pointer typedef for event handler to be sent to attached media */
typedef void (*DRV_MEMORY_EVENT_HANDLER)( MEMORY_DEVICE_TRANSFER_STATUS status, uintptr_t context );
/* Function pointer typedef to set the event handler with attached media */
typedef void (*DRV_MEMORY_DEVICE_EVENT_HANDLER_SET) ( const DRV_HANDLE handle, DRV_MEMORY_EVENT_HANDLER eventHandler, uintptr_t context );
typedef struct
{
DRV_MEMORY_DEVICE_OPEN Open;
DRV_MEMORY_DEVICE_CLOSE Close;
DRV_MEMORY_DEVICE_SECTOR_ERASE SectorErase;
DRV_MEMORY_DEVICE_STATUS Status;
DRV_MEMORY_DEVICE_READ Read;
DRV_MEMORY_DEVICE_PAGE_WRITE PageWrite;
DRV_MEMORY_DEVICE_EVENT_HANDLER_SET EventHandlerSet;
DRV_MEMORY_DEVICE_GEOMETRY_GET GeometryGet;
DRV_MEMORY_DEVICE_TRANSFER_STATUS_GET TransferStatusGet;
} DRV_MEMORY_DEVICE_INTERFACE;
Summary
Memory Device API Interface.
Description
This Data Structure is used by attached media to populate the required device functions for media transactions.
This will be used in memory driver init structure.
Remarks
None.