1.1.3.4.15 DRV_MEMORY_TransferStatusGet Function
C
MEMORY_DEVICE_TRANSFER_STATUS DRV_MEMORY_TransferStatusGet
(
const DRV_HANDLE handle
);Summary
Gets the current status of the transfer request on attached device.
Description
This routine gets the current status of the transfer request. The application must use this routine where the status of a scheduled request needs to be polled on.
The application can alternatively register a transfer handler to receive the transfer completion events.
Preconditions
DRV_MEMORY_Open() must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open function |
Returns
MEMORY_DEVICE_TRANSFER_ERROR_UNKNOWN
- If the handle is invalid
- If the status read request fails
MEMORY_DEVICE_TRANSFER_BUSY
- If the current transfer request is still being processed
MEMORY_DEVICE_TRANSFER_COMPLETED
- If the transfer request is completed
Example
// memoryHandle is the handle returned by the DRV_MEMORY_Open function.
if (MEMORY_DEVICE_TRANSFER_COMPLETED == DRV_MEMORY_TransferStatusGet(memoryHandle))
{
// Operation Done
}Remarks
This routine will block for hardware access. Used in Async mode of operation.