1.1.3.4.11 DRV_MEMORY_SyncWrite Function
C
bool DRV_MEMORY_SyncWrite
(
const DRV_HANDLE handle,
void *sourceBuffer,
uint32_t blockStart,
uint32_t nBlock
);Summary
Writes data for the specified number of memory blocks in Synchronous mode.
Description
This function schedules a blocking write operation for writing blocks of data into attached devices memory.
Preconditions
DRV_MEMORY_Open() routine must have been called to obtain a valid opened device handle. The memory block which has to be written, must have been erased before using the DRV_MEMORY_xxxErase() routine.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open function |
| sourceBuffer | The source buffer containing data to be programmed into media device memory |
| blockStart | Block start from where the data should be written to. |
| nBlock | Total number of blocks to be written. |
Returns
true
- If the transfer request is successfully completed.
false
- If the source buffer pointer is NULL
- If the client opened the driver for read only
- If the number of blocks to be written is either zero or more than the number of blocks actually available
- If the driver handle is invalid
Example
#define BUFFER_SIZE 4096 uint8_t writeBuffer[BUFFER_SIZE]; // Use DRV_MEMORY_GeometryGet () to find the write region geometry. uint32_t blockStart = 0x0; uint32_t nBlock = BUFFER_SIZE / block_size; // block_size for write geometry // memoryHandle is the handle returned by the DRV_MEMORY_Open function. if(DRV_MEMORY_SyncErase(memoryHandle, blockStart, nBlock) == false) { // Error handling here } if(DRV_MEMORY_SyncWrite(memoryHandle, &writeBuffer, blockStart, nBlock) == false) { // Error handling here }
Remarks
This API is supported only in RTOS environment.