1.1.3.4.2 DRV_MEMORY_Status Function
C
SYS_STATUS DRV_MEMORY_Status( SYS_MODULE_OBJ object );Summary
Gets the current status of the Memory driver module.
Description
This routine provides the current status of the Memory driver module.
Preconditions
Function DRV_MEMORY_Initialize should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| object | Driver object handle, returned from the DRV_MEMORY_Initialize routine |
Returns
SYS_STATUS_READY - Indicates that the driver is ready and accept requests for new operations.
SYS_STATUS_UNINITIALIZED - Indicates the driver is not initialized.
SYS_STATUS_BUSY - Indicates the driver is in busy state.
Example
SYS_MODULE_OBJ object; // Returned from DRV_MEMORY_Initialize SYS_STATUS MEMORYStatus; MEMORYStatus = DRV_MEMORY_Status(object);
Remarks
This routine will NEVER block waiting for hardware.