1.1.4.4.13 DRV_NAND_FLASH_SkipBlock_BlockTag Function
C
bool DRV_NAND_FLASH_SkipBlock_BlockTag(const DRV_HANDLE handle, uint16_t blockNum, bool badBlock)Summary
Tag NAND Flash block to bad or good.
Description
This routine tags given block of NAND Flash device to bad or good.
Preconditions
The DRV_NAND_FLASH_Open() routine must have been called for the specified NAND FLASH driver instance.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| blockNum | Block number to be tagged |
| badBlock | 1 - Block to be tagged as bad block. 0 - If block to be tagged as good block. |
Returns
true - If given block is tagged as bad or good
false - If failed to tag a block
Example
uint16_t blockNum = 0; DRV_HANDLE handle; // Returned from DRV_NAND_FLASH_Open if (DRV_NAND_FLASH_SkipBlock_BlockTag(handle, blockNum, 1)) // Block is tagged as bad }
Remarks
This routine will block for hardware access.