1.1.4.4.5 DRV_NAND_FLASH_ResetFlash Function
C
bool DRV_NAND_FLASH_ResetFlash(const DRV_HANDLE handle)Summary
Reset the flash device to standby mode.
Description
This function schedules a blocking operation for resetting the flash device to standby mode. All the volatile bits and settings will be cleared then, which makes the device return to the default status as power on.
Precondition
The DRV_NAND_FLASH_Open() routine must have been called for the specified NAND FLASH driver instance.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
Returns
true - Flash reset is completed successfully
false - Flash reset is failed
Example
DRV_HANDLE handle; // Returned from DRV_NAND_FLASH_Open
if(true != DRV_NAND_FLASH_ResetFlash(handle))
{
// Error handling here
}Remarks
This routine will block wait for hardware access.