1.1.4.4.12 DRV_NAND_FLASH_SkipBlock_BlockCheck Function
C
bool DRV_NAND_FLASH_SkipBlock_BlockCheck(const DRV_HANDLE handle, uint16_t blockNum)Summary
Checks whether NAND Flash block is bad or good.
Description
This routine returns false if the given block of NAND Flash device is bad otherwise true.
Preconditions
The DRV_NAND_FLASH_Open() routine must have been called for the specified NAND FLASH driver instance.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| blockNum | Block number to check |
Returns
true - If block is good
false - If block is bad
Example
uint16_t blockNum = 0;
DRV_HANDLE handle; // Returned from DRV_NAND_FLASH_Open
if (DRV_NAND_FLASH_SkipBlock_BlockCheck(handle, blockNum))
// Block is good
}Remarks
This routine will block for hardware access.