1.1.4.4.10 DRV_NAND_FLASH_GeometryGet Function
C
bool DRV_NAND_FLASH_GeometryGet( const DRV_HANDLE handle, DRV_NAND_FLASH_GEOMETRY *geometry );Summary
Returns the geometry of the NAND Flash device.
Description
This API gives the following geometrical details of the NAND Flash:
- deviceId (JEDEC Manufacturer ID)
- Bus Width
- Number of data bytes per page
- Number of spare bytes per page
- Block Size
- Device Size
- Number of logical units
- Number of bits of ECC correction
Precondition
The DRV_NAND_FLASH_Open() routine must have been called for the specified NAND FLASH driver instance.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| geometry | Pointer to destination geometry buffer into which geometry to be placed |
Returns
true - If geometry is successfully read from the NAND Flash
false - If geometry read is failed
Example
DRV_HANDLE handle; // Returned from DRV_NAND_FLASH_Open
DRV_NAND_FLASH_GEOMETRY nandFlashFlashGeometry;
if (DRV_NAND_FLASH_GeometryGet(handle, &nandFlashFlashGeometry))
{
// Geometry read successfully
}Remarks
This routine will block wait for hardware access.