1.1.4.4.11 DRV_NAND_FLASH_ParameterPageRead Function
C
bool DRV_NAND_FLASH_ParameterPageRead(const DRV_HANDLE handle, uint8_t *parameterPage, uint32_t size);Summary
Returns the Parameter page of the NAND Flash device.
Description
This routine reads the parameter page of the NAND Flash device. It reads target's organization, features, timings and other behavioural parameters of NAND Flash device.
Precondition
The DRV_NAND_FLASH_Open() routine must have been called for the specified NAND FLASH driver instance.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| parameterPage | Pointer to destination buffer into which parameter page to be placed from NAND Flash |
| size | Total number of parameter page data bytes to be read |
Returns
true - If parameter page is successfully read from the NAND Flash
false - If parameter page read is failed
Example
DRV_HANDLE handle; // Returned from DRV_NAND_FLASH_Open
uint8_t parameterPage[116];
if (DRV_NAND_FLASH_ParameterPageRead(handle, parameterPage, sizeof(parameterPage)))
{
// Parameter page read successfully
}Remarks
This routine will block wait for hardware access.