1.1.4.4.9 DRV_NAND_FLASH_FeatureGet Function
C
bool DRV_NAND_FLASH_FeatureGet(const DRV_HANDLE handle, uint8_t *featureData, uint8_t featureDataSize, uint8_t featureAddress)Summary
Read target specific features.
Description
This routine reads target specific features from NAND Flash.
Preconditions
The DRV_NAND_FLASH_Open() routine must have been called for the specified NAND FLASH driver instance.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| featureData | Pointer to destination buffer into which subfeature data to be placed from NAND Flash |
| featureDataSize | Total number of subfeature data bytes to be read |
| featureAddress | Specific feature address to be send after command cycle. |
Returns
true - If specific feature is read successfully from the flash
false - If invalid handle
Example
i.e. Read NAND Flash ECC controller if NAND Flash supports internal ECC controller #define NAND_FLASH_TARGET_DISABLE_INTERNAL_ECC 0x90 uint8_t featureData[4]; DRV_HANDLE handle; // Returned from DRV_NAND_FLASH_Open if (DRV_NAND_FLASH_FeatureGet(handle, featureData, sizeof(featureData), NAND_FLASH_TARGET_DISABLE_INTERNAL_ECC)) { // Feature data read successfully }
Remarks
This routine will block for hardware access.