1.1.4.4.15 DRV_NAND_FLASH_SkipBlock_BlockRead Function
C
bool DRV_NAND_FLASH_SkipBlock_BlockRead(const DRV_HANDLE handle, uint16_t blockNum, uint8_t *data, bool disableBlockCheck)Summary
Reads the data of a whole block from NAND Flash.
Description
This function schedules a blocking operation for reading the data of a whole block from NAND Flash.
Precondition
The DRV_NAND_FLASH_Open() routine must have been called for the specified NAND FLASH driver instance.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| blockNum | Block number to read |
| data | Pointer to destination data buffer |
| disableBlockCheck | 0 - Block will be checked as good before reading a given block. 1 - Block will not check before reading a given block. |
Returns
true - If Block read is successfully completed
false - If Block read fails
Example
DRV_HANDLE handle; // Returned from DRV_NAND_FLASH_Open uint16_t blockNum = 3; static uint8_t blockBuffer[262144 + 14336]; if (DRV_NAND_FLASH_SkipBlock_BlockRead(handle, blockNum, blockBuffer, 0)) { // Block read successfully completed }
Remarks
This routine will block waiting until read request is completed successfully.