1.1.4.4.4 DRV_NAND_FLASH_Status Function
C
SYS_STATUS DRV_NAND_FLASH_Status( const SYS_MODULE_INDEX drvIndex )Summary
Gets the current status of the NAND FLASH driver module.
Description
This routine provides the current status of the NAND FLASH driver module.
Preconditions
Function DRV_NAND_FLASH_Initialize should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| drvIndex | Identifier for the instance used to initialize driver |
Returns
SYS_STATUS_READY - Indicates that the driver is ready and accept requests for new operations.
SYS_STATUS_UNINITIALIZED - Indicates the driver is not initialized.
SYS_STATUS_BUSY - Indicates the driver is in busy state.
Example
SYS_STATUS Status; Status = DRV_NAND_FLASH_Status(DRV_NAND_FLASH_INDEX);
Remarks
This routine will NEVER block wait for hardware.