1.1.4.4.17 DRV_NAND_FLASH_SkipBlock_PageRead Function
C
bool DRV_NAND_FLASH_SkipBlock_PageRead(
const DRV_HANDLE handle,
uint16_t blockNum,
uint16_t pageNum,
uint8_t *data,
uint8_t *spare,
bool disableBlockCheck
);Summary
Reads the data and/or the spare area of a page of given block from NAND Flash.
Description
This function schedules a blocking operation for reading the data and/or the spare area of a page of given block from NAND Flash.
Precondition
The DRV_NAND_FLASH_Open() routine must have been called for the specified NAND FLASH driver instance.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| blockNum | Block number to read page from |
| pageNum | Page number to read inside the given block |
| data | Pointer to destination data buffer |
| spare | Pointer to destination spare buffer. |
| disableBlockCheck | 0 - Block will be checked as good before reading a page. 1 - Block will not check before reading a page. |
Returns
true - If Page read is successfully completed
false - If Page read fails
Example
DRV_HANDLE handle; // Returned from DRV_NAND_FLASH_Open uint16_t blockNum = 3; uint16_t pageNum = 0; static uint8_t pageBuffer[4096 + 224]; if (DRV_NAND_FLASH_SkipBlock_PageRead(handle, blockNum, pageNum, pageBuffer, 0, 0)) { // Page read successfully completed }
Remarks
This routine will block waiting until read request is completed successfully.