1.3.2.3.2 MAC_WRP_Open Function
C
MAC_WRP_HANDLE MAC_WRP_Open (
const SYS_MODULE_INDEX index,
MAC_WRP_BAND band
);Summary
Opens the specified MAC Wrapper instance and returns a handle to it.
Description
This routine opens the specified MAC Wrapper instance and provides a handle that must be provided to all other client-level operations to identify the caller and the instance of the module.
Precondition
Function MAC_WRP_Initialize must have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| index | Index for the instance to be opened |
| band | Working band for PLC (should be inline with the hardware) |
Returns
If successful, the routine returns a valid open-instance handle (a number identifying both the caller and the module instance). If an error occurs, the return value is MAC_WRP_HANDLE_INVALID.
Example
MAC_WRP_HANDLE handle; SYS_MODULE_OBJ sysObjMacWrp; // Populate initData if needed sysObjMacWrp = MAC_WRP_Initialize(G3_MAC_WRP_INDEX_0); handle = MAC_WRP_Open(G3_MAC_WRP_INDEX_0, MAC_WRP_BAND_CENELEC_A); if (handle == MAC_WRP_HANDLE_INVALID) { // Handle error }
Remarks
This routine must be called before any other MAC Wrapper API function, except MAC_WRP_Initialize.