1.3.2.3.13 MAC_WRP_SetRequestSync Function
C
MAC_WRP_STATUS MAC_WRP_SetRequestSync
(
MAC_WRP_HANDLE handle,
MAC_WRP_PIB_ATTRIBUTE attribute,
uint16_t index,
const MAC_WRP_PIB_VALUE *pibValue
);Summary
The MAC_WRP_SetRequestSync primitive sets the value of an attribute in the MAC layer Parameter Information Base (PIB).
Description
SetRequestSync primitive is used to set the value of a PIB. Sync suffix indicates that result of set operation is provided upon function call return, in the return status code.
Precondition
A valid handle has to be obtained before calling this function, by means of MAC_WRP_Open function.
Parameters
| Param | Description |
|---|---|
| handle | A valid handle which identifies the Mac Wrapper instance |
| attribute | Identifier of the Attribute to provide value. See MAC_WRP_PIB_ATTRIBUTE |
| index | Index of element in case Attribute is a table. Otherwise index must be set to '0' |
| pibValue | Pointer to MAC_WRP_PIB_VALUE object where value is contained |
Returns
Result of set operation as a MAC_WRP_STATUS code.
Example
// ... MAC_WRP_HANDLE handle; handle = MAC_WRP_Open(G3_MAC_WRP_INDEX_0, MAC_WRP_BAND_CENELEC_A); // ... MAC_WRP_STATUS status; const MAC_WRP_PIB_VALUE value = { .length = 1, .value = 6 }; status = MAC_WRP_SetRequestSync(handle, MAC_WRP_PIB_MAX_FRAME_RETRIES, 0, &value); if (status == MAC_WRP_STATUS_SUCCESS) { // PIB correctly set }
Remarks
None.