1.3.2.3.55 MAC_WRP_POS_ENTRY_RF Struct
C
typedef struct __attribute__((packed))
{
MAC_WRP_SHORT_ADDRESS shortAddress;
uint8_t forwardLqi;
uint8_t reverseLqi;
uint8_t dutyCycle;
uint8_t forwardTxPowerOffset;
uint8_t reverseTxPowerOffset;
uint16_t posValidTime;
} MAC_WRP_POS_ENTRY_RF;Summary
The MAC RF POS Table Entry as defined in the G3-PLC standard.
Description
This structure contains the fields that define a MAC RF POS table entry as defined in the G3-PLC standard. POS table contains an entry for every node we have received a frame, either addressed for us or not.
Field description:
- shortAddress. Short Address of node in our hearing domain.
- forwardLqi. Link Quality reported by neighbour when receiving our frames.
- reverseLqi. Link Quality of last received frame from node.
- dutyCycle. Current Duty Cycle consumed by neighbour node.
- forwardTxPowerOffset. TxPowerOffset used to transmit to neighbour node.
- reverseTxPowerOffset. TxPowerOffset used by neighbour node when transmitting towards us.
- posValidTime. Time left, in seconds, for the entry to expire.
Remarks
It is only used when RF MAC layer is present.