1.3.2.3.18 MAC_WRP_ScanRequest Function
C
void MAC_WRP_ScanRequest
(
MAC_WRP_HANDLE handle,
MAC_WRP_SCAN_REQUEST_PARAMS *scanParams
);Summary
The MAC_WRP_ScanRequest primitive sets MAC layer(s) in Network Scan mode.
Description
Scan operation asks MAC layer(s) to send a Beacon Request frame and wait for incoming Beacon frames. During the Scan period, Beacons received will be notified by means of MAC_WRP_BeaconNotifyIndication callback. Result is provided in the corresponding Confirm callback.
Precondition
A valid handle has to be obtained before calling this function, by means of MAC_WRP_Open function.
Parameters
| Param | Description |
|---|---|
| handle | A valid handle which identifies the Mac Wrapper instance |
| scanParams | Pointer to structure containing required parameters for request. See MAC_WRP_SCAN_REQUEST_PARAMS |
Returns
None.
Example
// ... MAC_WRP_HANDLE handle; handle = MAC_WRP_Open(G3_MAC_WRP_INDEX_0, MAC_WRP_BAND_CENELEC_A); // ... MAC_WRP_SCAN_REQUEST_PARAMS params = { .scanDuration = 15 }; MAC_WRP_ScanRequest(handle, ¶ms); // Wait for Scan Confirm
Remarks
None.