1.3.2.3.10 MAC_WRP_DataIndication Typedef
C
typedef void (*MAC_WRP_DataIndication)(MAC_WRP_DATA_INDICATION_PARAMS *diParams);
Summary
Pointer to a Data Indication Event handler function.
Description
This data type defines the required function signature for the MAC Wrapper Data Indication event handling callback function. A client must register a pointer using the event handling function whose function signature (parameter and return value types) matches the types specified by this function pointer in order to receive Data Indication events back from module.
Parameters
| Param | Description |
|---|---|
| diParams | Pointer to structure containing parameters related to Indication. See MAC_WRP_DATA_INDICATION_PARAMS |
Returns
None.
Example
App_DataIndication(MAC_WRP_DATA_INDICATION_PARAMS *params)
{
// Check addressing
if (params->destPanId == myPanId)
{
if (params->destAddress.addressMode == MAC_WRP_ADDRESS_MODE_SHORT)
{
if (params->destAddress.shortAddress == myShortAddress) {
// Frame is for me
}
}
else if (params->destAddress.addressMode == MAC_WRP_ADDRESS_MODE_EXTENDED)
{
if (params->destAddress.extendedAddress == myExtendedAddress) {
// Frame is for me
}
}
}
}Remarks
None.