1.3.2.3.65 MAC_WRP_TONE_MASK Struct
C
typedef struct
{
uint8_t toneMask[(MAC_WRP_MAX_TONES + 7) / 8];
} MAC_WRP_TONE_MASK;Summary
Defines the G3 Tone Mask at Mac Wrapper level.
Description
Tone Mask is a bitmap in which each bit represents one of the carriers present in the PLC work band (36 carriers in CEN-A, 16 carriers in CEN-B, 72 carriers in FCC). '1' indicates the carrier is used, '0' indicates the carrier is not used.
Field description:
- toneMask. Array of bytes containing the bitmap explained above.
Remarks
It is only used when PLC MAC layer is present.