4.4.3.8.1.13 SOTSB – Start
Of Telegram Status for Path B
Note:
- Set to hardware-controlled read-only mode if the get_rx_telegram state
machine is active.
| Name: | SOTSB |
| Offset: | 0x091 |
| Reset: | 0x00 |
This register
displays the status of all start of telegram conditions. The corresponding bit is set to
‘1’ if the condition has matched. It is cleared if a
‘1’ is written to its position or the receiving path B is disabled
(RDPR.PRFLT = 1 or RDPR.PRPTB = 1). The flags are
handled by the hardware if the get_rx_telegram state machine (SSMRR.SSMR) is activated.
In this case, the flags are cleared if an activated error condition for RDSIFR.EOTB
occurs. This is done automatically by toggling the RDPR.APRPTB
bit.
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
| | WCOAO | RROB | SFIDOB | WUPOB | MANOB | SYTOB | AMPOB | CAROB | |
| Access | R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W | |
| Reset | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | |
Bit 7 – WCOAO Wake Check OK on
Path A OK
The bit is set at a successful
wake check OK from path A (RDSIFR.WCOA) that can be used as a precondition for a
successful wake check (RDSIFR.WCOB) and start of telegram (RDSIFR.SOTB) detection on
path B. It is cleared if a ‘1’ is written to its position, a
‘1’ is written to the RDSIFR.SOTB interrupt flag, or the
receiving path B is disabled.
Bit 6 – RROB RSSI Range OK on
Path B
This bit is set if the
received signal strength on path B is within the expected range. The RSSI comparison
is based on the first averaged RSSI sample after RX start-up. A failure of this
check is indicated by the setting of the RSSFB flag in the EOTSB register. It is
cleared if a ‘1’ is written to its position, a ‘1’
is written to the RDSIFR.SOTB interrupt flag, or the receiving path B is
disabled.
Bit 5 – SFIDOB Start of Frame
Identifier Matched on Path B
This bit indicates a
successful correlator-based start of frame ID check. It is cleared if a
‘1’ is written to its position, a ‘1’ is
written to the RDSIFR.SOTB interrupt flag, or the receiving path B is
disabled.
Bit 4 – WUPOB Wake-Up Pattern
Matched on Path B
This bit is set if the wake-up
pattern match occurred. It is cleared if a ‘1’ is written to its
position, a ‘1’ is written to the RDSIFR.SOTB interrupt flag, or
the receiving path B is disabled.
Bit 3 – MANOB Manchester Coding
OK on Path B
This bit is set if the
manchester coding check is OK. The manchester coding is verified for the duration
specified in the SYCSB register. If it was right for this duration, it is considered
OK. A failure of this check is indicated by the setting of the MANFEB flag in the
EOTSB register. It is cleared if a ‘1’ is written to its position,
a ‘1’ is written to the RDSIFR.SOTB interrupt flag, or the
receiving path B is disabled.
Bit 2 – SYTOB Symbol Timing OK on
Path B
This bit is set if the symbol
timing check is OK. The symbol timing is verified for the duration specified in the
SYCSB register. If it was right for this duration, it is considered OK. A failure of
this check is indicated by the setting of the SYTFEB flag in the EOTSB register. It
is cleared if a ‘1’ is written to its position, a
‘1’ is written to the RDSIFR.SOTB interrupt flag, or the
receiving path B is disabled.
Bit 1 – AMPOB Amplitude OK on
Path B
This bit is set if the signal
amplitude inside the demodulator is above a specified threshold (DMMB.DMATB). A
failure of this check is indicated by the setting of the AMPFB flag in the EOTSB
register. It is cleared if a ‘1’ is written to its position, a
‘1’ is written to the RDSIFR.SOTB interrupt flag, or the
receiving path B is disabled.
Bit 0 – CAROB Carrier Check OK on
Path B
This bit is set by a
successful signal carrier check. A failure of this check is indicated by the setting
of the CARFB flag in the EOTSB register. It is cleared if a ‘1’ is
written to its position, a ‘1’ is written to the RDSIFR.SOTB
interrupt flag, or the receiving path B is disabled.