4.4.3.8.1.2 RDPR – RX DSP Power Reduction Register
This register is used to disable the clocks for several parts of the RX DSP path.
Each block with a disabled clock is automatically put into reset state. A gradual
power reduction scheme allows a step-by-step enabling of the blocks and a fast
restart of the required blocks. A disabled block has no active clock source and a
reset is executed in the internal registers. The external settings of the block are
preserved. Enabling the power reduction at the beginning of the RX path disables and
resets all subsequent circuits to assure consistent operation. A push synchronizer
is used to transfer the settings from the AVR clock domain to the asynchronous
receive path. The user has to carry out the following procedure to modify the
registers: Check that the RDPR register is not busy (RDPR.RDPRF =
0). Write a new configuration to the RDPR register. The data is
taken by the register and transferred to the Rx_DSP block. The RDPR.RDPRF flag is
HIGH while this operation is running, indicating that further writing is blocked.
The settings are active and can be modified again when the operation is complete
(RDPR.RDPRF = 0).
- Data can be written to this
register only if RDPR.RDPRF =
0. This is because a handshake is activated whenever data is written to RDPR, and RDPR.RDPRF =1indicates that the procedure is not completed yet. It is required to wait until RDPR.RDPRF becomes ‘0’. The only way to abort the procedure is to disable and reset the complete RX DSP block by setting RDCR.RDEN =0. - The bits in this register are
reset (in addition to the normal resets) if RDCR.RDEN =
0.
| Name: | RDPR |
| Offset: | 0x004 |
| Reset: | 0x00 |
| Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
| RDPRF | ARDPRF | APRPTA | APRPTB | PRTMP | PRFLT | PRPTA | PRPTB | ||
| Access | R | R | R | R | R/W | R/W | R/W | R/W | |
| Reset | 0 | 0 | 0 | 0 | 1 | 1 | 1 | 1 |
Bit 7 – RDPRF RX DSP Power Reduction Register (RDPR) Busy Flag
| Value | Description |
|---|---|
0 | IDLEMode: The circuit is ready to start an update cycle. Writing new settings to the RDPR register is possible. |
1 |
The RDPR is performing an update cycle. Writing to RDPR is blocked until the setting is transferred to the RX DSP block. |
Bit 6 – ARDPRF Automatic RX DSP Power Reduction Flag
Bit 5 – APRPTA Automatic Power Reduction of Path A
0 and
PRPTA = 0. ARPTA is temporarily set to HIGH and back to LOW if the
automatic mode is enabled (DMCRA.DMARA = 1) and an EOTA condition
becomes true.Bit 4 – APRPTB Automatic Power Reduction of Path B
0 and
PRPTB = 0. ARPTB is temporarily set to HIGH and back to LOW if the
automatic mode is enabled (DMCRB.DMARB = 1) and an EOTB condition
becomes true.Bit 3 – PRTMP Power Reduction Register for Temperature Measurement
| Value | Description |
|---|---|
0 | Clock for temperature measurement is running. |
1 | Clock for temperature measurement is disabled. |
Bit 2 – PRFLT Power Reduction Register for the Digital Channel Filter
| Value | Description |
|---|---|
0 | Channel filter is enabled. The clocks are running. |
1 | Channel filter and the subsequent blocks (demodulator and receiving path A and path B) are disabled by stopping the clocks. A reset of the internal registers and the corresponding clock dividers is performed. |
Bit 1 – PRPTA Power Reduction Register for Receiving Path A
0 and APRPTA = 0. The behavior of the ARPTA
bit depends on the DMCRA.DMARA configuration.0.| PRPTA | DMARA | Description |
|---|---|---|
0 | 0 | The receiving path A is enabled. The demodulator, frame synchronizer and RX buffer are running. |
0 | 1 | Receiving path A is in automatic restart mode. Path A is receiving until an enabled EOT condition occurs. A hardware-controlled reset with subsequent restart is performed. This mode is useful for repeated attempts to find a signal on the same frequency. |
1 | x | Receiving path A is disabled. The demodulator, clock recovery, symbol timing check, frame synchronizer and RX buffer are disabled by stopping their clocks. A reset of the internal registers and the corresponding clock dividers is performed. The external settings for the circuits are preserved to allow a fast restart. |
Bit 0 – PRPTB Power Reduction Register for Receiving Path B
0 and APRPTB = 0. The behavior of the ARPTB
bit depends on the DMCRB.DMARB configuration.0.| PRPTB | DMARB | Description |
|---|---|---|
0 | 0 | The receiving path B is enabled. The demodulator, frame synchronizer and RX buffer are running. |
0 | 1 | Receiving path B is in automatic restart mode. Path B is receiving until an enabled EOT condition occurs. A hardware-controlled reset with subsequent restart is performed. This mode is useful for repeated attempts to find a signal on the same frequency. |
1 | x | Receiving path B is disabled. The demodulator, clock recovery, symbol timing check, frame synchronizer and RX buffer are disabled by stopping their clocks. A reset of the internal registers and the corresponding clock dividers is performed. The external settings for the circuits are preserved to allow a fast restart. |