1.3.5.4.10 CL_NULL_RedirectResponse Function
C
void CL_NULL_RedirectResponse
(
uint16_t conHandle,
uint8_t *eui48,
uint8_t *data,
uint16_t dataLen
);
Summary
Response to a direct connection establishment indication.
Description
This routine is used to respond to a direct connection establishment indication.
Precondition
The CL_NULL_Initialize routine must have been called before.
Parameters
| Param | Description |
|---|---|
| conHandle | Unique identifier of the connection |
| eui48 |
Pointer to the address of the node to which this connection will be "redirected" |
| data | Data associated with the connection establishment procedure |
| dataLen | Length of the data in bytes |
Returns
None.
Example
uint8_t eui48[6];
memset(eui48, 0x12, 6);
CL_NULL_RedirectResponse(8, eui48, NULL, 0);
Remarks
None.