1.3.5.4.3 CL_NULL_EstablishRequest Function
C
void CL_NULL_EstablishRequest
(
uint8_t *eui48,
uint8_t type,
uint8_t *data,
uint16_t dataLen,
uint8_t arq,
uint8_t cfBytes,
uint8_t ae
);
Summary
Request a connection establishment.
Description
This routine is used to request a connection establishment.
Precondition
The CL_NULL_Initialize routine must have been called before.
Parameters
| Param | Description |
|---|---|
| eui48 |
Pointer to the address of the node to which this connection will be addressed |
| type | Convergence Layer type of the connection |
| data | Data associated with the connection establishment procedure |
| dataLen | Length of the data in bytes |
| arq |
Flag to indicate whether or not the ARQ mechanism should be used for this connection |
| cfBytes |
Flag to indicate whether or not the connection should use the contention or contention-free channel access scheme |
| ae |
Flag to indicate that authentication and encryption is requested (v1.4) |
Returns
None.
Example
uint8_t eui48[6];
memset(eui48, 0x12, 6);
CL_NULL_EstablishRequest(eui48, 9, NULL, 0, 1, 0, 0);
Remarks
The result of the request is returned in the confirm callback.