1.3.5.4.1 CL_NULL_Initialize Function
C
void CL_NULL_Initialize(void);
Summary
Initializes the PRIME Null Convergence Sublayer.
Description
This routine initializes the PRIME Null Convergence Sublayer.
Precondition
The MAC_Initialize function should have been called before calling this function.
Parameters
None.
Returns
None.
Example
CL_NULL_Initialize();
Remarks
This routine is normally not called directly by an application. It is called by the PRIME Stack initialization routine.