1.3.5.4.28 CL_432_Initialize Function
C
void CL_432_Initialize(void);
Summary
Initializes the PRIME 4-32 Convergence Sublayer.
Description
This routine initializes the PRIME 4-32 Convergence Sublayer.
Precondition
None.
Parameters
The MAC_Initialize function should have been called before calling this function.
Returns
None.
Example
CL_432_Initialize();
Remarks
This routine is normally not called directly by an application. It is called by the PRIME Stack initialization routine.