1.3.5.4.23 CL_NULL_MlmeMpDemoteRequest Function
C
void CL_NULL_MlmeMpDemoteRequest(uint8_t lsid);
Summary
Request to trigger a demotion process in a Service Node that is in a Switch functional state and supports MultiPHY promotion.
Description
This routine is used to request to trigger a demotion process in a Service Node that is in a Switch functional state and supports MultiPHY promotion.
Precondition
The CL_NULL_Initialize routine must have been called before.
Parameters
| Param | Description |
|---|---|
| lsid | Local switch identifier |
Returns
None.
Example
CL_NULL_MlmeMpDemoteRequest(125);
Remarks
The result of the request is returned in the confirm callback.
This primitive only applies in PRIME v1.4.