1.3.5.4.5 CL_NULL_ReleaseRequest Function
C
void CL_NULL_ReleaseRequest
(
uint16_t conHandle
);
Summary
Request to release a connection.
Description
This routine is used to request a connection release.
Precondition
The CL_NULL_Initialize routine must have been called before.
Parameters
| Param | Description |
|---|---|
| conHandle |
Unique identifier of the connection |
Returns
None.
Example
CL_NULL_ReleaseRequest(3);
Remarks
The result of the request is returned in the confirm callback.