1.3.5.4.45 CL_432_ReleaseRequest Function
C
void CL_432_ReleaseRequest
(
uint16_t dstAddress
);
Summary
Request to release a CL-432 connection.
Description
This routine is used to request a CL-432 connection release.
Precondition
The CL_432_Initialize routine must have been called before.
Parameters
| Param | Description |
|---|---|
| dstAddress |
Address to disconnect |
Returns
None.
Example
CL_432_ReleaseRequest(300);
Remarks
The result of the request is returned in the confirm callback.