29.2.2 __builtin_add_32

Description

Add shifted value to accumulator. Although the hardware type of an accumulator is wider than the natural size of int, the compiler uses the shorter type as the expected use of the value will eventually be in the natural int type. Note, that this type can be different based on architecture. 

Example:

volatile register int result asm("A");
int32_t value;

result = __builtin_add_32(result, value, 0);

Prototype

int __builtin_add_32(int Accum, int32_t value, const int32_t shift);

Arguments

Accum - Accumulator to add

value - value to add

shift - amount to shift value before being added to Accum

Return Value

Adds the possibly shifted value to Accum and returns the same value.

Machine Instruction

add

Error Messages

An error message is reported if the shift value is outside of the range supported by the target device.