29.2.31 __builtin_fmal
Description
__builtin_fmal computes (x * y) + z as if with
unlimited range and precision, rounding only once to the result format. This can provide
more accurate results than performing the multiplication and addition separately,
especially with floating-point numbers. This function operates on 64-bit,
double-precision floating-point numbers. For more information, see 9.3 Floating-Point Data Types.
Prototype
long double __builtin_fma(long double x, long double y, long double z)
;
Arguments
x - value to be multiplied by the multiplier
y - value of multiplier
z - value to add to the result of the
multiplication
Return Value
Returns value of the mathematical and rounding operations. See also 4.3.4.1 Why Are My Floating-Point Results Not Quite What I Am Expecting?
Machine Instruction
mac.d
Error Messages
An error message is reported if there is a floating-point exception.