29.2.79 __builtin_write_ACCH

Description

Write a value to the high part of an accumulator. If loading the entire accumulator, this function or __builtin_lac should be executed first.

Example:

volatile register int Accum asm("A");
int value;
 
Accum = __builtin_write_ACCH(value);

Prototype

int __builtin_write_ACCH(int value);

Arguments

value - value to write

Return Value

Accumulator is updated by writing the high part of the accumulator; the low part of the accumulator is cleared and the value is sign extended to the upper part of the accumulator.

Machine Instruction

lac.l

Error Messages

None.