29.2.26 __builtin_flim_32

Description

Force (Signed) Data Range Limit. Simultaneously compares a 32-bit signed data value to a maximum signed limit value and a minimum signed limit value.

If the data value is greater than the maximum, the data value is set to the maximum value.

If the data value is less than the minimum, the data value is set to the minimum value.

If the data value is within the maximum-minimum values, the data value is not changed.

Prototype

int32_t __builtin_flim(int32_t value, int32_t high, int32_t low);

Arguments

value – Data value

high – Maximum limit value

low – Minimum limit value

Return Value

Returns value clamped between high and low.

Machine Instruction

flim.l

Error Messages

None