5.3.5.8 Unbond Device (U,<1-8,Z>)
Format:
U,<1-8,Z>
Command U removes existing bonding. This command works in both central
or peripheral GAP roles.
Command U expects one input parameter. The parameter indicates the index of the
bonding that needs to be removed. Use command LB to determine the index
of the bonding. If the input parameter is the letter Z, then all
bonding information is cleared. If an empty index is available, the new pairing and
bonding information is added at the first available empty index.
| Example: | U,1 | // Remove the bond with index 1 |
| Response: | AOK
| // Success |
Err | // Syntax error or invalid parameter |