5.3.5.5 Add Bonded List Into Accept List (JB)
Format:
JB
Use command JB to add all currently bonded devices to the accept list.
Command JB does not expect any parameter.
The random address in the accept list can be resolved with command JB for
connection purpose. If the peer device changes its resolvable random address, the RNBD451 module is still able to detect that the
different random addresses are from the same physical device and, therefore, allows a
connection from such a peer device. This feature is particularly useful if the peer
device is an iOS or Android device that uses a resolvable random address.
| Default | None | |
| Example: | JB
| // Add all bonded devices to accept list |
| Response: | AOK
| // Success |