5.3.5.9 List All Bonded Devices (LB)
Format:
LB
Command LB lists all bonded devices in the following format:
<index>,<address>,<address type>
where <index> is a single-digit index in the range of 1-8, representing the index of the
bonded device in the bonding table. Use this index in command
C<1-8> to reconnect and in command
U,<1-8> to remove bonding.
The <address> is a six-byte number representing the address of the bonded device;
<address type> is a single-digit number, taking either ‘0’ or
‘1’. Value ‘0’ for <address type> means that
the address in the bonding information is a public address. In such a case, use command
C or C<1-8> to reconnect to the bonded
device. Value ‘1’ for <address type> means a random address;
therefore, reconnection is not possible using the bonded information because the peer
device may use a different random address when the RNBD451 module tries to reconnect.
| Example: | LB
| // List all bonded devices |