5.2.23 Set HCI Determination (SH,<0,1>)
Format: SH,<0,1>
This command is used to enable/disable the determining scheme to enter HCI mode:
- 1: enable HCI mode determining scheme
- 0: disable HCI mode determining scheme
The determining scheme is to check the first command format to judge if the RNBD451 module is in HCI mode or RN application after reboot. When the RNBD451 module enters HCI mode, it will be recorded into PDS and invalidate the determining scheme. The GH command can retrieve the setting.
| Example: | SH,1 | // Enable HCI mode determining scheme |
| Response: | AOK | // Success |
Err | // Syntax error or invalid parameter |
Note: The command is supported in RNBD451 v1.1 and later.