5.2.8 Get Configuration (G<char>)
Format:
G<char>
This command displays the stored settings for a command where <char> is a
command name (S prefix command).
| Example: | GA
| // Return to Authentication mode set by command
SA |
| Response: | 2 | // Value of the settings, the setting of SA is 2 for
example |