5.2.4 Enter Command Mode ($$$)
Format:
$$$
This command makes the RNBD451 module enter Command mode
and display the command prompt. The device passes the characters as data, and enters the
Command mode if it sees the $$$ sequence. If the Command mode guard
bit is set using the SR command, the device checks if there are any
bytes before or after the $$$ characters in a one-second window, the
device does not enter Command mode, and these bytes are passed through. For more details
on SR command, refer to Set Application Options (SR,<hex16>).
The user can change the character string used to enter Command mode using the S$ command. For more details on S$ command, refer to Set Enter Command Character (S$,<char>).
The UART receives a CMD> prompt indicating the start of a command
session.
| Example: | $$$
| // Enter Command mode |
| Response: | CMD>
| // If command prompt is enabled |